Locating Positioning
INDEXING PLUNGERS
A device or system used to position and move objects or parts in a specific sequence within a manufacturing or assembly process. It has an internal spring system, its function is to fix a position by means of a pin located at the tip.
Applications
Some of the sectors in which indexers are used are:
- Electronics: In the manufacture of electronic products, such as cell phones, computers, storage devices and electronic components, indexers are used for precise positioning of parts, soldering, assembly and testing.
- Food and beverage: Used for sorting, labeling, packaging, bottle filling, packing and other operations related to food and beverage production.
As well as in Packaging, Automotive, Pharmaceutical, among others.
MISUMI inCAD Library
Example No.000237
The assembly shown corresponds to one of the
mechanisms of a workstation.
In this section an indexer is used to maintain the
position of a cylinder that can be positioned by means
of notches.



Types of Indexers
More commercial model.
Only required to be mounted on a threaded surface, can be selected with stop or with free return.
This model is commonly used for applications where higher pressure is required.
This model tends to have greater visibility and has a larger contact area.
This model does not have a knob, it is selected when the customer wishes to install an existing one or under another geometry.
This model is side mounted, depending on the type of application and available space.

Location Bushing
We have the location bushings for the indexers, hardened and easy to install.

M
M Thread and pitch. Ranges from M3 to M20
B
Pin diameter
S
Pin race
Materials and Finishes
We have options available in the most commercial metallic materials used in the industry for their properties:
- Carbon steel: selected for low handling.
- Stainless steel: ideal for humid environments.
We also handle different options that cover a quite high range in terms of protection of the components against the different harmful elements in the environment such as dust, humidity or corrosion.
| Material | Surface finish | Features |
|---|---|---|
| Carbon steel | Pavonado | It provides a black color appearance and greatly improves its corrosion resistance. |
| Electrodeless nickel plating | It gives a silvery yellowish appearance and improves its resistance to corrosion, but to a lesser extent than bluing. | |
| Nickel plating | It provides a silver-colored appearance and greatly enhances its corrosion resistance. Its selection may depend on taste in appearance or standards. | |
| Trivalent chrome plating | Provides a silver-colored appearance greatly improves its corrosion resistance. Their selection may depend on taste in appearance or standards. |
Main Advantages
- Excellent for positioning Easy to
- Use and assemble
- Variety of materials and threads
- Wide variety of shapes and sizes
MISUMI Benefits
- Configurable components
Standard and globally valid part number 3D
- 2D/3D CAD download in different formats (STEP, SolidWorks, CATIA, Inventor, AutoCAD)
- Preview


- Quotations and direct purchases from our online store
Related Products