Caster, Leveling & Cabinet Hardware
LEVERS
Also known as clamping handles, there are levers used to hold or fix components, boards, etc. Ergonomically designed to make it easier to grip and improve user comfort.
Applications
Levers are used in a wide variety of industrial applications:
- Industrial machinery and equipment: Used to control and operate various industrial machines and equipment, such as presses, stamping machines, packaging machines, and cutting and forming machinery
- Valves and Control Systems: Levers are commonly used to operate valves in piping and fluid systems, such as ball valves, gate valves, and butterfly valves.
- Robotics and automated handling: In process automation, levers are used to control the movements of industrial robots, robotic arms, and automated handling systems on production lines.
- Conveyors and Movement Systems: Levers are used to control the movement and speed of conveyors and conveyor belts in production and distribution lines.
MISUMI inCAD Library
Example CLDMC6-12B
The assembly shown corresponds to a Fixture / Fastening tooling.
Its objective is to position and hold the production part to later
install attachments, laterally you will find the levers which help
a quick change if you need to install a tool with another
production part number.


Types

With male rope

Threaded

Y-type

Double arm / Butterfly

Cam
More commercial.
Only mounting on a threaded surface is required, but mounting will exert pressure.
It is selected when there is already a threaded shaft,
this model is added to be able to manipulate the system.
Compact and mostly manipulated with the fingers, in the previous models the hand is used.
Very similar to type Y, it is defined at the customer’s
discretion.
These levers are used to exert greater pressure. Its
function is very similar to that of a clamp.

Tension lever
It is used to manipulate large mechanisms, where a greater contact area is required to exert a greater moment.
COLORS
Color is one of the most important aspects, since these play a very important function within the industry, visual safety. According to the type or standard used in a process or production plant, the color indicates a safety code, for example: Red (prohibited), yellow (caution/warning), orange (machinery danger), etc.


Measures and Materials
MEASURES
The main measure to consider is the string (M) and its
length (L) for levers with screws or those that are
threaded.

MATERIALS
Steel: It is the most economical option, selected for low handling
or exposure to humidity.
Zinc alloy: Selected for moderate handling and exposure to moisture..
Stainless steel: Selected for humid environments or those exposed to liquids.
Nylon: Selected for high handling, reduces friction to the touch.
APPLICATION
The clamping levers have an internal spring mechanism,
this helps initially to exert pressure and to be able to rotate
to choose the position of the handle without ceasing to exert
pressure.

SURFACE TREATMENT
MISUMI Benefits
- Configurable components
Standard and globally valid part number 3D
- 2D/3D CAD download in different formats (STEP, SolidWorks, CATIA, Inventor, AutoCAD)
- Preview


- Quotations and direct purchases from our online store
Related Products