Caster, Leveling & Cabinet Hardware
LEVELING MOUNTS
It is a device for machinery that is used to level an object or machine that is being installed and when the ground is uneven. Also reduce vibrations to avoid low product quality and equipment damage.
Applications
Leveling mounts are used in a wide variety of industrial applications and here are some examples:
- Production lines: Used in automated production lines to ensure that parts or products are at the proper level before moving on to the next stage of the process. This is essential to ensure accurate manufacturing and avoid problems such as misalignment and product damage.
- Industrial Robotics: Industrial robots often require level surfaces to perform precise tasks. Leveling mounts are used to adjust the height of the platforms on which the robots work, thus ensuring that the movements and operations of the robots are consistent and accurate.
- Automated assembly and assembly: In the manufacture of complex products, Leveling mounts are used to adjust the height of automated assembly and assembly stations. This allows parts to be precisely aligned, which in turn improves the quality of the final product and reduces the need for rework.
- CNC Machinery: On Computer Numerical Control (CNC) machines, leveling mounts are essential to ensure that the worktable is perfectly level. This ensures precision in the machining of parts and components.
MISUMI inCAD Library
Example FJGMS10-75-R
It is a manual mechanism that releases several parts at once.
The leveling mounts support the structure.


Types
MISUMI’s leveling mounts are configurable, which makes them adaptable to the specific needs of your application.
This includes shaft length, special machining, custom ends, materials, finishes, among others.
Standard leveling mounts, has its respective base and screw.
It is used in heavy loads and supports the entire weight of the machine or base.
Used in leveling when the adjustment is not vertical.
It has an internal bearing and is used for heavy
loads.
Used when vibration reduction is
required.

For instruments
measurement

Anchor
Used in laboratories where greater rectification is
These leveling mounts have holes to fix on the ground.

Diameter (D)
from 14 to 300mm
Screw length (A)
from 25 to 1000mm
Rope size (M)
M5 to M45
Load capacity (N)
from 0.98kN to 330kN
Rotating angle (e)
from 7.5º to 40º
Materials and Finishes
Leveling mounts can be made from a variety of materials, depending on application requirements and operating conditions.

- Steel
- Stainless steel
- Resin

- Steel
- Stainless steel
- Resin * Rubbers

- Resin
- Rubbers
- Urethanes
The metallic surface is refined, eliminating marks and scratches.
Cover the surface to prevent oxidation and wear, by means of an alkaline solution.
A chrome layer is applied which provides hardness and resistance to wear and corrosion.
The piece is immersed in a layer of zinc and offers
protection against corrosion.
Protects the part from corrosion.
It has an appearance similar to zinc and offers resistance to corrosion and wear.
MISUMI Benefits
- Configurable components
Standard and globally valid part number 3D
- 2D/3D CAD download in different formats (STEP, SolidWorks, CATIA, Inventor, AutoCAD)
- Preview


- Quotations and direct purchases from our online store
Related Products